Digital input and output status information
|
Data format |
Primary VIFE |
Manufacturer specific VIFE |
Description |
||
|---|---|---|---|---|---|
|
bin |
hex |
bin |
hex |
||
|
03 |
E001 1011 |
1B |
— |
— |
Digital input control mode:
|
|
05 |
— |
— |
E010 1111 |
2F |
Pulse constant (pulses/unit) |
|
02 |
— |
— |
E011 0010 |
32 |
Digital input status:
NOTE: This information only applies if the digital input
control mode is set to Input Status.
|
|
03 |
— |
— |
E011 0000 |
30 |
Digital input association with partial energy data reset
|
|
03 |
— |
— |
E010 1100 |
2C |
Energy pulse duration in milliseconds NOTE: This information
only applies if the digital output mode is set to energy pulsing.
|
|
05 |
— |
— |
E010 1110 |
2E |
Pulse weight of the digital output NOTE: This information
only applies if the digital output mode is set to energy pulsing.
|
|
03 |
E001 1010 |
1A |
— |
— |
Digital output control mode
|
|
03 |
— |
— |
E010 1101 |
2D |
Digital output association with energy pulsing:
|
|
02 |
— |
— |
E011 0110 |
36 |
Digital output association with overload alarm:
|