Mechanical characteristics
|
Characteristic |
Value |
Meters |
||
|---|---|---|---|---|
|
IP degree of protection |
Front panel |
IP40 |
iEM3100 / iEM3200 / iEM3300 series |
|
|
Meter body |
IP20 |
iEM3100 / iEM3200 series |
||
|
Meter body except bottom wiring surface |
IP20 |
iEM3300 series |
||
|
Impact rating |
IK08 |
iEM3100 / iEM3200 / iEM3300 series |
||
|
Active energy display range |
In kWh or MWh up to 99999999 MWh |
iEM3200 series |
||
|
In kWh: 8 + 1 digits up to 99999999.9 |
iEM3100 / iEM3300 series |
|||
|
Energy pulsing LED (yellow *) |
500 imp/k(W/VAR)h |
iEM3100 series |
||
|
5000 imp/k(W/VAR)h without consideration of transformer ratios |
iEM3200 series |
|||
|
200 imp/k(W/VAR)h |
iEM3300 series |
|||