DOCA0005EN-15

Meter Setup and Status

Address

Register

Action
(R/W/WC)

Size

Type

Units

Description

0x07D3

2004

R

2

UInt32

Second

Meter Operation Timer

NOTE: Not applicable for iEM3150 / iEM3250 / iEM3350

0x07DD

2014

R

1

UInt16

Number of Phases

0x07DE

2015

R

1

UInt16

Number of Wires

0x07DF

2016

R/WC

1

UInt16

Power System:

  • 0 = 1PH2W L-N
  • 1 = 1PH2W L-L
  • 2 = 1PH3W L-L with N
  • 3 = 3PH3W
  • 11 = 3PH4W
  • 13 = 1PH4W multi L with N

0x07E0

2017

R/WC

1

UInt16

Hz

Nominal Frequency

0x07E8

2025

R

1

UInt16

Number VTs

NOTE: Not applicable for iEM3150 / iEM3155 / iEM3350 / iEM3355

0x07E9

2026

R/WC

2

Float32

V

VT Primary

NOTE: Not applicable for iEM3150 / iEM3155 / iEM3350 / iEM3355

0x07EB

2028

R/WC

1

UInt16

V

VT Secondary

NOTE: Not applicable for iEM3150 / iEM3155 / iEM3350 / iEM3355

0x07EC

2029

R/WC

1

UInt16

Number CTs

NOTE: Not applicable for iEM3150 / iEM3155 / iEM3350 / iEM3355

0x07ED

2030

R/WC

1

UInt16

A

CT Primary

NOTE: Not applicable for iEM3150 / iEM3155 / iEM3350 / iEM3355

0x07EE

2031

R/WC

1

UInt16

A

CT Secondary

NOTE: Not applicable for iEM3150 / iEM3155 / iEM3350 / iEM3355

0x07F3

2036

R/WC

1

UInt16

VT Connection Type:

  • 0 = Direct Connect
  • 1 = 3PH3W (2 VTs)
  • 2 = 3PH4W (3 VTs)

NOTE: Not applicable for iEM3150 / iEM3155 / iEM3350 / iEM3355

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?