DOCA0005EN-15

Configuring basic communications settings

Before communicating with the meter using M-Bus protocol, use the HMI to configure the following settings:

Setting

Possible values

Baud rate

  • 300
  • 600
  • 1200
  • 2400
  • 4800
  • 9600

Primary address

1 – 250

NOTE: For M-Bus communication, the device consumes 2 standard loads (2 Unit Loads or 2UL).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?