DOCA0005EN-15

Overview

The meter does not contain any user-serviceable parts. If the meter requires service, contact your local Schneider Electric representative.

NOTICE
RISK OF DAMAGE TO THE METER
  • Do not open the meter case.
  • Do not attempt to repair any components of the meter.
Failure to follow these instructions can result in equipment damage.

Do not open the meter. Opening the meter voids the warranty.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?