DOCA0005EN-15

Digital output

Programmable (energy pulsing or overload alarm): iEM3135 / iEM3155 / iEM3165 / iEM3235 / iEM3255 / iEM3265 / iEM3335 / iEM3355 / iEM3365

Pulse output: iEM3110 / iEM3210 / iEM3310

The pulse output indicates the primary consumption with consideration of transformer ratios.

It can be directly connected to a 24 V DC (< 30 V DC) input on a Zelio or Twido PLC.

For other concentrators, if V DC / Rin > 15 mA, add a resistor Radd = (V DC / 0.01) - Rin Ω

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?