DOCA0005EN-15

The front panel display in configuration mode

The image below illustrates the various elements of the display in configuration mode:

A

Parameter

B

Setting

C

Indicates that the setting impacts the Multi Tariff feature

D

Configuration mode icon

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?