DOCA0005EN-15

Instantaneous (RMS) measurements

Object ID

Units

Default COV

Object name / description

7

A

50

AI07 - Current Phase 1

8

A

50

AI08 - Current Phase 2

9

A

50

AI09 - Current Phase 3

10

A

50

AI10 - Current Average

11

V

10

AI11 - Voltage L1-L2

12

V

10

AI12 - Voltage L2-L3

13

V

10

AI13 - Voltage L3-L1

14

V

10

AI14 - Voltage Average L-L

15

V

10

AI15 - Voltage L1-N

16

V

10

AI16 - Voltage L2-N

17

V

10

AI17 - Voltage L3-N

18

V

10

AI18 - Voltage Average L-N

19

kW

10

AI19 - Active Power Phase 1

20

kW

10

AI20 - Active Power Phase 2

21

kW

10

AI21 - Active Power Phase 3

22

kW

10

AI22 - Active Power Total

23

kVAR

AI23 - Reactive Power Total

24

kVA

10

AI24 - Apparent Power Total

25

0.2

AI25 - Power Factor Total

26

Hz

10

AI26 - Frequency

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?