DOCA0005EN-15

Data display screens: iEM3135 / iEM3155 / iEM3165 / iEM3175 / iEM3235 / iEM3255 / iEM3265 / iEM3275 /iEM3335 / iEM3355 / iEM3365 / iEM3375

 

A

Import / export indicated for total active (Ea) and total reactive (Er) energy. Other energy measurements are import only

 

B

Resets all energy measurements except total active energy and total reactive energy

 

C

Diagnosis screen appears if there is a specific event

     

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?