DOCA0005EN-15

Digital Input (iEM3155 / iEM3255 / iEM3355)

Address

Register

Action
(R/W/WC)

Size

Type

Units

Description

0x1C69

7274

R

1

UInt16

Digital Input Control Mode:

  • 0 = Normal (Input Status)
  • 2 = Multi Tariff Control
  • 3 = Input Metering
  • 5 = All Energy Reset

0x22C8

8905

R

2

Bitmap

Digital Input Status (only Bit 1 is used):

  • Bit 1 = 0, relay open
  • Bit 1 = 1, relay closed

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.