DOCA0005EN-15

Digital input setup

Function profile

UCPT

Struct Members

Range / Options

Description

nciCfgDigitInpt

UCPTDigitalInput

0, 1

Associates the digital input to reset partial energy data:

  • 0 = Digital input is not associated with the partial energy reset.
  • 1 = Digital input is associated with the partial energy reset.

Setting this property to 1 also updates nciDICtrlMode (UCPTDiCtrlMode) to All Energy Reset

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?