DOCA0005EN-15

Communications Setup

Command Number

Action
(R/W)

Size

Type

Unit

Range

Description

5000

W

1

UInt16

(Reserved)

W

1

UInt16

(Reserved)

W

1

UInt16

(Reserved)

W

1

UInt16

1 – 247

Address

W

1

UInt16

0, 1, 2

Baud Rate:

  • 0 = 9600
  • 1 = 19200
  • 2 = 38400

W

1

UInt16

0, 1, 2

Parity:

  • 0 = Even
  • 1 = Odd
  • 2 = None

W

1

UInt16

(Reserved)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?