DOCA0005EN-15

iEM3100 and iEM3300 series

Functions

Advantages

Can directly measure feeders up to:

  • iEM3100 series: 63 A
  • iEM3300 series: 125 A

Embedded current transformers (CTs)

Saves installation time and space in the cabinet

No wiring to manage

Clear distribution network

Adapted to be installed with Acti9 iC60 (iEM3100 series) or Acti9 C120, NG125 (iEM3300 series) circuit breakers

Can be used in three-phase systems with or without neutral

Can be used for single-phase multi-circuit monitoring

3 single feeders can be monitored with a single meter

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?