Multi Tariff setup
|
Function profile |
UCPT |
Struct Members |
Range / Options |
Description |
|---|---|---|---|---|
|
nciCfgCommTariff |
UCPTTariffMode |
— |
0, 1 |
Set Multi Tariff control mode to Disabled or by Communication
NOTE: To configure the Multi Tariff feature to be controlled
by the digital input or device clock, use the HMI.
|
|
nciCfgTariffSel |
UCPTTariffSelect |
— |
1, 2, 3, 4 |
Set the active tariff
NOTE: You can only set the tariff using this method if the Tariff
Mode is set to by Communication.
|