DOCA0005EN-15

Configuration menu for iEM3135 / iEM3155 / iEM3165 / iEM3175 / iEM3335 / iEM3355 / iEM3365 / iEM3375

 

A

Not available on iEM3175 / iEM3375

 

B

iEM3155 / iEM3355

 

C

iEM3135 / iEM3335

 

D

iEM3165 / iEM3365

     

Section

Parameter

Options

Description

Wiring

Type

  • 3PH4W
  • 1PH2W L-N
  • 1PH2W L-L
  • 1PH3W L-L-N
  • 3PH3W
  • 1PH4W Multi L-N

Select the power system type the meter is wired to.

Frequency

Frequency

  • 50
  • 60

Select the frequency of the electrical power system, in Hz.

Date

Date

DD-MMM-YYYY

Set the current date using the specified format.

Time

Time

hh:mm

Set the time using the 24-hour format.

Multi Tariffs

Control Mode

  • Disable
  • by Communication
  • by Digital Input
  • by Internal Clock

Select the tariff control mode:

  • Disable: the Multi Tariff function is disabled.

  • by Communication: the active tariff is control by communications. See the chapter for the applicable protocol for more information.

  • by Digital Input: the digital input is associated with the Multi Tariff function. A signal to the digital input changes the active tariff.

  • by Internal Clock: the device clock controls the active tariff. If you set the Control Mode to by Internal Clock, you must also configure the schedule. Set the time when each tariff period starts, using the 24 hour clock format (00:00 to 23:59). The start time of the next tariff is the end time of the current tariff. For example, T2 start equals the end of T1.

Overload Alarm

Alarm

  • Disable
  • Enable

Select whether or not the Overload Alarm is enabled:

  • Disable: the alarm is disabled.

  • Enable: the alarm is enabled. If you enabled the Overload Alarm, you must also configure the Pick Up Value in kW from 1 - 9999999.

Digital Output (Not available on iEM3175 / iEM3375)

DO Function

  • Disable
  • Alarm
  • Pulse (kWh)
  • Pulse (kVARh)

Select how the digital output functions:

  • Disable: the digital output is disabled.

  • Alarm: the digital output is associated with the overload alarm. In the event of trigger, the digital output remains in the ON state until the alarm drop out point is crossed.

  • Pulse (kWh): The digital output is associated with energy pulsing (active energy). When this mode is selected, you can select the energy parameter and set the Pulse Constant (imp/kWh) and the Pulse Width (ms).

  • Pulse (kVARh): The digital output is associated with energy pulsing (reactive energy). When this mode is selected, you can select the energy parameter and set the Pulse Constant (imp/kVARh) and the Pulse Width (ms).

Digital Input

DI Function

  • Input Status
  • Tariff Control
  • Input Metering
  • Partial Reset

Select how the digital input functions:

  • Input status: the digital input records the status of the input, for example, OF, SD of a circuit breaker.

  • Tariff Control: the digital input is associated with the Multi Tariff function. A signal to the digital input changes the active tariff.

  • Input Metering: the digital input is associated with input metering. The meter counts and records the number of incoming pulses. If you set the DI Function to Input Metering, you must also configure In. Pulse Constant.

  • Partial Reset: a signal to the digital input initiates a partial reset.

LED Energy Pulse

Energy

  • kWh
  • kVARh

Set the active energy and reactive energy.

Communication (iEM3155 / iEM3355)

Slave Address

1 – 247

Set the address for this device. The address must be unique for each device in a communications loop.

Baud Rate

  • 19200
  • 38400
  • 9600

Select the speed for data transmission. The baud rate must be the same for all devices in a communications loop.

Parity

  • Even
  • Odd
  • None

Select None if the parity bit is not used. The parity setting must be the same for all devices in a communications loop.

NOTE: Number of stop bits = 1.

Communication (iEM3135 / iEM3335)

Primary Addr.

0 – 255

Set the address for this device. The address must be unique for each device in a communications loop.

Baud Rate

  • 2400
  • 4800
  • 9600
  • 300
  • 600
  • 1200

Select the speed for data transmission. The baud rate must be the same for all devices in a communications loop.

Communication (iEM3165 / iEM3365)

MAC Addr.

1 – 127

Set the address for this device. The address must be unique for each device in a communications loop.

Baud Rate

  • 9600
  • 19200
  • 38400
  • 57600
  • 76800

Select the speed for data transmission. The baud rate must be the same for all devices in a communications loop.

Device ID

0 – 4194303

Set the Device ID for this device. Make sure the Device ID is unique in your BACnet network.

Com.Protection

Com.Protection

  • Enable
  • Disable

Protects selected settings and resets from configuration via communications.

Contrast

Contrast

1 – 9

Increase or decrease the value to increase or decrease the display contrast.

Password

Password

0 – 9999

Sets the password for accessing the meter configuration screens and resets.

Reset Config

Reset Config

Settings are reset to their defaults, except for Password. Meter restarts.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?