DOCA0189EN–05

Assembly Installation of LC1G265–500 Contactor and Overload Relay on Plate

After assembling LC1G265–500 contactor and LR9G500 overload relay (see Assembly Procedure), perform the following procedure to mount the assembly on the plate:

  1. Drill 6 holes in the plate. Maximum hole diameter: 6 mm (0.23 in.)

    NOTE: To ease the mounting, drilling stencils JYT1902701 can be downloaded from the www.se.com website.
  2. Insert the two short screws (A) half way diagonally on the plate.

  3. Place the contactor and overload relay on the short screw heads.

  4. Tighten the two short screws with PZ2 screwdriver at the right torque.

  5. Insert the two long screws (B) diagonally through the contactor and another two screws to fix the overload relay and then tighten them at the right torque.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.