80459-641-01, Rev. 09

Configuring with PowerSuite Software

The PowerSuite Software kit contains one PowerSuite CD, one USBtoRS485 converter, and one 10 ft. (3 m) cable.

  1. Install the PowerSuite software on your PC.

  2. Set the top switch on the converter to 0-TER MULT.

  3. Set the Polarization switch on the side of the converter to OFF.

  4. Connect one end of the cable to the RJ-45 port on the converter.

  5. Connect the other end of the cable to the TeSys T controller.

  6. Connect the USB connector on the converter to a USB port on your PC. (The converter uses the UniTelway/Modbus driver that is included with PowerSuite.)

  7. Set the full load current (FLC)

    1. Go to Settings -> Thermal -> FLC1 (OC1)

    2. Enter FLC1 as a % of FLCmax.

  8. Convert the amperes to FLC Settings

    1. FLC values are stored as a percentage of FLCmax in the TeSys T:
      FLC (in %) = FLC (in A) / FLCmax

      NOTE: For details about the PowerSuite software, refer to the TeSys T LTM R Motor Management Controller User Manual specific to your network communication protocol. Verify the proper configuration of the TeSys T controller per your application.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?