80459-641-01, Rev. 09

Space Requirements

Install MCCs in an area with a minimum of 3 ft. (0.9 m) of free space in front of front-of-board construction. An additional 3 ft. (0.9 m) is necessary in the rear of back-to-back construction. This free space provides adequate room to remove and install units. (More space may be required for some applications; refer to applicable local and national installation codes.) Provide at least 0.5 in. (13 mm) of space between the back of front-of-board MCCs and a wall. For damp locations, provide at least 6 in. (152 mm).

When selecting a location for the installation of an MCC, carefully consider accessibility, overhead clearances, and future expansions. Considering these factors will eliminate many difficulties during this and future MCC installations.

NOTE: Model 6 MCCs with the arc-rated option have pressure-relief roof flaps for top venting of arc fault gases. These MCCs require a minimum of 28.5 in. (724 mm) from the top plate of the MCC to the nearest obstruction (minimum ceiling height of 10 ft. (3 m) including base channel). See Required Obstruction-Free Area concerning the required clearance above the equipment.
DANGER
Burn hazard from HOT GASES
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E, NOM-029-STPS-2011, or CSA Z462.
  • Keep the area directly above the equipment clear and unobstructed for a distance of 28.5 in. (724 mm) from the roof.
Failure to follow these instructions will result in death or serious injury.

The shaded area (Required Obstruction-Free Area) above the arc-rated MCC must be free from obstructions.

Required Obstruction-Free Area

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?