80459-641-01, Rev. 09

Configuring with HMI

The HMI may be supplied either as a unit-mounted option, or as a separate, handheld programming kit containing one HMI and one 3.3 ft. (1 m) connection cable.

  1. Connect the HMI to the TeSys T unit:

    1. If supplied as a unit-mounted option, the connection will be made at the factory.

      or

    2. Connect the programming kit directly to the ‘LTME or HMI’ port on the front of theTesys T controller.

      or

    3. Connect the programming kit via the optional, unitmounted RJ-45 port.
  2. Input Full Load Current (FLC):

    1. Using the HMI, go to Menu>Protection Settings>Thermal>Thermal Overload>FLC1

      NOTE: For additional details, refer to the TeSys T LTM CU Control Operator Unit User’s Manual and the TeSys T LTM R Motor Management Controller User's Manual specific to your network communication protocol. (See iMCC-Related Literature for the document numbers.)
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?