80459-641-01, Rev. 09

iMCC Communications

NOTICE
LOSS OF COMMUNICATIONS
  • Do not use excessive force when making cabling connections.
  • Connections are keyed to ensure that pins are properly aligned.
Failure to follow these instructions can result in equipment damage.

Before energizing the equipment, check the items below to verify that the iMCC networking and cabling are set up and connected properly.


  • Cabling Connections

  • Verify that the network length without a repeater is less than 1500 feet (457 m).

  • Verify that the MCC cables are connected between shipping splits. See Cables Between Shipping Splits for instructions.

  • Verify that each device tap cable is properly connected to the main trunk line.

  • Verify that all network connections are secure.

  • Verify that terminating resistors are installed as required per network protocol.


Communications Setup

  • Verify that all devices have been assigned correct addresses; see Device Addressing for specific addressing parameters.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?