80459-641-01, Rev. 09

Horizontal Bus Barriers

  1. Remove the screw located at the top of the two-piece bus barriers.

  2. Remove the screw located at the bottom of the two-piece bus barriers.

  3. Pull the two metal barriers out of the MCC and discard them.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?