80459-641-01, Rev. 09

Non-Seismic Applications

Fasten each section to the floor (see Standard Base Channel Mounting) using 1/2 in. or 3/4 in., grade 5 or higher, bolts, and flat washers (furnished by customer).

0.88 in. (22 mm) diameter base channel mounting holes provide clearance for bolt expansion anchors for 1/2 in. bolts.

NOTE: Although sections are free-standing, floor fastening prevents movement, thereby preventing conduit connection damage.

Standard Base Channel Mounting

Base Channel Mounting For 18-Pulse AC Drive MCC Sections

A Structure anchoring locations (typical of 4)
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?