80459-641-01, Rev. 09

Removal

  1. Turn off all power supplying this equipment before working on or inside the equipment, and follow lockout/tagout procedures. Always use a properly rated voltage sensing device to confirm the power is off.

  2. A captive rivet at the bottom of each bus barrier panel secures the panels to mounting brackets on the MCC (see Fixed Horizontal Bus Barrier below, and Horizontal Bus Barrier Installation and Removal and Barrier Installed and Removed).

    Fixed Horizontal Bus Barrier

  3. Firmly grasp the head of the left side rivet and pull until the rivet releases from the mounting bracket.

  4. Pull out on the bottom of the left side panel until the tab at the top of the panel is clear of the top track (see Horizontal Bus Barrier Installation and Removal).

  5. Remove the panel from the MCC.

  6. Repeat steps 3–5 for the right side panel.

Horizontal Bus Barrier Installation and Removal

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?