80459-641-01, Rev. 09

Receiving the MCC

Inspect the MCC for damage as soon as it is received. Delivery of the equipment to a carrier at any of the Schneider Electric plants or other shipping point constitutes delivery to the purchaser. Title and all risk of loss or damage in transit shall pass to the purchaser at that time. Refer to the Schneider Electric Conditions of Sale for more details. All claims for loss and damage must be made by the purchaser to the carrier.

If the packaging material is removed, replace it for protection until the MCC is installed.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?