80459-641-01, Rev. 09

Installation

  1. Turn off all power supplying this equipment before working on or inside the equipment, and follow lockout/tagout procedures. Always use a properly rated voltage sensing device to confirm the power is off.

  2. Insert the tab on the right side panel into the top track on the right side of the MCC and set it into place (see Fixed Horizontal Bus Barrier and Horizontal Bus Barrier Installation and Removal).

  3. Secure the right side panel by pushing the rivet firmly into the hole of the mounting bracket.

  4. Repeat steps 2 and 3 for the left side panel.

Barrier Installed and Removed

Installed Removed
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?