Motor Logic Plus Remote Programming
Remote programming can be used for setpoint programming and data acquisition purposes. Follow the steps below to remotely configure the Motor Logic Plus overload. (See Command Line Codes for a description of the command line codes referenced in the steps.)
-
Stop the overload by sending code “02H” to the command register (C6H).
-
If network programming has not been enabled, send code “05H” to the command register.
-
Program the appropriate parameter. See Motor Logic Plus Address Descriptions (Read only, all registers are 16-bit words) for a register map with a list of parameters. For more detailed information, refer to Schneider Electric instruction bulletin 30072-013-102_. See Read-Only Registers and Read/Write Registers to determine the location and addressing of parameters within the Motor Logic Plus register map.
-
Restart the overload by using code “01H.”
Command Line Codes
Code | Command |
---|---|
01H | Start/reset |
02H | Stop |
03H | Display lock |
04H | Display unlock |
05H | Network program enable |
06H | Network program disable |
07H | Network watchdog enable* |
08H | Network watchdog disable* |
Motor Logic Plus Address Descriptions (Read only, all registers are 16-bit words)
Address | Code | Description | Notes | |
---|---|---|---|---|
RAM | Relative* | |||
A0 | 1A0 | VOLTAV | Average voltage L–L | V~ |
A2 | 1A1 | IAVE | Raw average current | A (x100, x10, x1), multiplied by scale factor |
A4 | 1A2 | VUB | Voltage unbalance | 0–100% |
A6 | 1A3 | IUB | Current unbalance | 0–100% |
A8 | 1A4 | PFANGLE | Power factor angle | Degrees |
AA | 1A5 | CAPTY | Thermal capacity remaining | 0–100% |
AC | 1A6 | GFC | Ground fault current | A (x100, x10, x1), multiplied by scale factor |
AE | 1A7 | ERCODE/TRIPRN | Real time event (RTE) and trip indicator (TI) | 8-bit nibble-coded RTE; 8-bit coded TI |
B0 | 1A8 | FH | Event history | Event order: 4th, 3rd, 2nd, Last |
B2 | 1A9 | PID | Manufacture year/model and scale | 8-bit year; 8-bit ID and scale |
B4 | 1AA | VA-C | Line voltage A–C | V~ |
B6 | 1AB | VB-C | Line voltage B–C | V~ |
B8 | 1AC | VA-B | Line voltage A–B | V~ |
BA | 1AD | IC | Raw current phase C | A (x100, x10, x1), multiplied by scale factor |
BC | 1AE | IB | Raw current phase B | A (x100, x10, x1), multiplied by scale factor |
BE | 1AF | IA | Raw current phase A | A (x100, x10, x1), multiplied by scale factor |
C0 | 1Bo | RD1 | Remaining restart delay RD1 | |
C2 | 1B1 | RD2 | Remaining restart delay RD2 | |
C4 | 1B2 | RD3 | Remaining restart delay RD3 | |
C6 | 1B3 | COMLINE | Command line code (address C6H) | see Table 12 (write only) |
C8 | 1B4 | Scale | PowerLogic scale parameter (read only) | 0, 1, 2; 16-bit signed word (2’s complement, read only) |
CA | 1B5 | LV | Under-voltage threshold | 170 V~ to HV (600 V~ model; 450 V~ to HV) |
CC | 1B6 | HV | Over-voltage threshold | LV to 528 V~ (600 V~ model; LV to 660 V~) |
CE | 1B7 | VUB | Voltage unbalance threshold | 2–15%, or 999 (off) |
D0 | 1B8 | MULT | Effective turns ratio | Determined by model |
D2 | 1B9 | OC | Overcurrent threshold | Current range of SSOLR |
D4 | 1BA | UC | Undercurrent threshold | 0.5 x OC Min. to OC Max., Off |
D6 | 1BB | CUB | Current unbalance threshold | 2–25%, or 999 (off) |
D8 | 1BC | TC | Overcurrent trip class | 5, J5, 10, J10, 15, J15, 20, J20,
30, J30 (J = Jam protection is enabled) |
DA | 1BD | RD1 | Rapid cycle timer | 2–500 s |
DC | 1BE | RD2 | Restart delay RD2 | 2–500 min. |
DE | 1BF | RD3 | Restart delay RD3 | 2–500 min. |
E0 | 1C0 | #RU | Restarts after UC | 0, 1, 2, 3, 4, A |
E2 | 1C1 | #RF | Number of restarts | 0, 1, oc1, 2, oc2,
3, oc3, 4, oc4, A, ocA (0 = manual, A = continuous, oc = automatic restart after RD2 expires) |
E4 | 1C2 | UCTD | Undercurrent trip delay | 2–60 s |
E6 | 1C3 | GF | Ground fault threshold | 0.15 x OC Min. to 0.2 x OC Max., Off |
E8 | 1C4 | ADDR | RS-485 slave address | 01–99 |
Read-Only Registers
RAM Address | Relative Address* | Code | Description | Notes | ||
---|---|---|---|---|---|---|
A0 | 1A0 | VOLTAV | Average voltage L-L | Volts | ||
A2 | 1A1 | IAVE | Raw average current | A (x100, x10, x1), multiplied by scale factor | ||
A4 | 1A2 | VUB* | Voltage unbalance | 0–100% | ||
A6 | 1A3 | IUB* | Current unbalance | 0–100% | ||
A8 | 1A4 | PFANGLE* | Power factor angle | Degrees | ||
AA | 1A5 | CAPTY* | Thermal capacity remaining | 0–100% | ||
AC | 1A6 | GFC* | Ground fault current | A (x100, x10, x1), multiplied by scale factor | ||
AE | 1A7 | ERCODE/TRIPRN | Bit-real time messages and trip indicator | Bit # | TRIPRN | ERCODE |
0 | Event lockout | Under-voltage | ||||
1 | Remote stop | Over-voltage | ||||
2 | Contactor event | Unbalance voltage | ||||
3 | Under current | Under current | ||||
4 | Over current | Phase reversal | ||||
5 | Ground fault | Unbalance current | ||||
6 | Current unbalance | Single phase voltage > 25% | ||||
7 | Current single phase > 50% unbalance | Single phase current > 50% | ||||
B0 | 1A8 | FH* | NIBBLE_CODED -4 event history | The four-event history is based on the
following scheme: 16 15 14 13 12 11 10 9 8 7 6 5 4 3 2 1, where bits 1–4 = Last event, bits 5–8 = 2nd last event, bits 9–12 = 3rd last event, and bits 13–16 = 4th last event. These four bits indicate a hex value that corresponds to the following events: |
||
1 | Over-voltage | |||||
2 | Under-voltage | |||||
3 | N/A | |||||
4 | Contactor misoperation | |||||
5 | Phase reversal | |||||
6 | Single phase | |||||
7 | Ground fault | |||||
8 | Current unbalance | |||||
9 | Remote off command | |||||
10 | Overcurrent | |||||
11 | Undercurrent | |||||
B2 | 1A9 | PID* | Manufacture year, month, product type/scale | 8-bit year, 4-bit month, 4-bit I/O and scale | ||
B4 | 1AA | VA-C | Line voltage A–C | Volts | ||
B6 | 1AB | VB-C | Line voltage B–C | Volts | ||
B8 | 1AC | VA-B | Line voltage A–B | Volts | ||
BA | 1AD | IC | Raw current phase C | A (x100, x10, x1), multiplied by scale factor | ||
BC | 1AE | IB | Raw current phase B | A (x100, x10, x1), multiplied by scale factor | ||
BE | 1AF | IA | Raw current phase A | A (x100, x10, x1), multiplied by scale factor | ||
C0 | 1B0 | RD1* | Remaining restart delay RD1 | Seconds | ||
C2 | 1B1 | RD2* | Remaining restart delay RD2 | Seconds | ||
C4 | 1B2 | RD3* | Remaining restart delay RD3 | Seconds |
Read/Write Registers
RAM Address | Relative Address | Code | Description | Range | Default | |
---|---|---|---|---|---|---|
C6 | 1B3 | COM-LINE | Command Line* | Reset/run/stop, display lock, network configuration enable | Motor Logic Plus Command Register (C6 hex) | |
01H | Start/reset | |||||
02H | Stop | |||||
03H | Display lock | |||||
04H | Display unlock | |||||
05H | Network program enable | |||||
06H | Network program disable | |||||
C8 | 1B4 | Scale | PowerLogic scale parameter | 0, 1, 1–2; 16-bit signed word (2s complement, read only) | Model dependent | |
CA | 1B5 | LV | Low voltage threshold | 170 V (450 V*) - HV setting | 435 | |
CC | 1B6 | HV | Over-voltage threshold | LV setting - 528 V (660 V*) | 500 | |
CE | 1B7 | VUB | Voltage unbalance threshold | 2–15% or 999% | 5% | |
D0 | 1B8 | MULT | CT/turns effective ratio | 1 or 10–200 | 1 | |
D2 | 1B9 | OC | Overcurrent threshold | OL current range | Min. rating | |
D4 | 1BA | UC | Undercurrent threshold | 0.5 x OC Min. to OC Max., Off | 0.8 x OC Min. | |
D6 | 1BB | CUB | Current unbalance threshold | 2–25% or 999% | 6% | |
D8 | 1BC | TC | Overcurrent trip class | 5, J5, 10, J10, 15, J15, 20, J20, 30,
J30 (J = Jam protection is enabled) |
5 | 5 decimal |
J5 | 133 decimal | |||||
10 | 10 decimal | |||||
J10 | 138 decimal | |||||
15 | 15 decimal | |||||
J15 | 143 decimal | |||||
20 | 20 decimal | |||||
J20 | 148 decimal | |||||
30 | 30 decimal | |||||
J30 | 158 decimal | |||||
DA | 1BD | RD1 | Rapid cycle timer | 2–500 seconds | 10 | |
DC | 1BE | RD2 | Restart delay all events except undercurrent | 2–500 minutes | 8 | |
DE | 1BF | RD3 | Restart delay after undercurrent | 2–500 minutes | 20 | |
E0 | 1C0 | #RU | # Restarts after undercurrent | 0, 1, 2, 3, 4, A (Automatic) | RU Values | |
8.1 | 0–4 in decimal | |||||
8.2 | A = 255 decimal | |||||
E2 | 1C1 | #RF | # Restarts all events except undercurrent | 0, 1, oc1, 2, oc2, 3, oc3, 4, oc4, A,
ocA (0 = manual, A = continuous, oc = automatic restart after RD2 expires) |
RF Values | |
0 | 1 decimal | |||||
1 | 2 decimal | |||||
oc1 | 3 decimal | |||||
2 | 4 decimal | |||||
oc2 | 5 decimal | |||||
3 | 6 decimal | |||||
oc3 | 7 decimal | |||||
4 | 8 decimal | |||||
oc4 | 9 decimal | |||||
A | 10 decimal | |||||
ocA | 11 decimal | |||||
E4 | 1C2 | UCTD | Undercurrent trip delay | 2–60 seconds | 5 | |
E6 | 1C3 | GF | Ground fault current threshold | (0.4) AOL current range or Off | 0.15 x Min. | |
E8 | 1C4 | ADDR | RS-485 slave address | 01–99 | 1 |