Sprinkler-Resistant Low Voltage MCC Pull Box
Refer to Removing the Lifting Angles and Hardware for the following steps.
-
Uninstall and discard the lifting angles (A) by removing the 3/8-in bolts and washers (B) securing them.
-
Remove and discard the top closing plate (C) from the MCC section by removing the 10-32 screws (D) securing it.
NOTE: For main sections with ArcBlok™ technology, do not remove the top closing plate (C) since the pull box will be installed over it. Remove only the 10-32 screws (D).Refer to Installing the Pull Box.
-
Remove the front panel (E) from the pull box (F) by removing the 10-32 screws (G) securing it.
-
Position the pull box on top of the MCC section frame (for standard sections) or on top of the closing plate (for main sections with ArcBlok technology).
NOTE: The overhang located at the top of the pull box must be facing the front of the MCC section. -
Install the two 3/8-in bolts and washers (B) removed in step 1. Place them through the pull box lower side channels and into the top of the MCC section.
-
Re-install the pull box front panel removed in step 3.
-
Remove the two 10-32 screws (H) located on the side of the pull box near the bottom.
-
Remove the two 10-32 screws, 3/8-in bolt, and washer located on the top closing plate of the adjacent MCC section (I).
-
Install the pull box splice angle (J) re-using the hardware removed in steps 7 and 8.