80459-641-01, Rev. 09

Introduction

Model 6 Motor Control Centers that are seismically certified have been certified to the seismic requirements of the listed regional building codes and/or seismic design standards per the manufacturer’s certificate of compliance (CoC). Equipment labels and CoCs are provided with all seismically certified Model 6 Motor Control Centers. Refer to the equipment CoC for certification details and applicable seismic parameters. To maintain the validity of this certification, the installation instructions provided in this section must be followed.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?