80459-641-01, Rev. 09

Aligning the MCC

A smooth, level surface must be provided for installation. An uneven foundation may cause misalignment of shipping blocks, units, and doors. The surface under an MCC must be of a non-combustible material, unless bottom plates are installed in each vertical section.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?