80459-641-01, Rev. 09

Installation

NOTE: The horizontal bus barrier contains two identical panels with arrows at the top. The “handle” on the left panel faces the front of the MCC section. The “handle cavity” on the right panel faces the front of the MCC section (see Right Panel (Side View)).
  1. Align the arrows on the right panel and top track as shown in Installing the Right Panel into the Rear Groove.

  2. Lift the panel up into the rear groove of the top track.

  3. Lower the panel into the rear groove of the bottom track.

  4. Slide the panel to the far right.

  5. Align the arrows on the left panel and top track.

  6. Repeat Steps 2 and 3 using the left panel and front groove.

  7. Slide the panel to the left until it locks (snaps) into place.

  8. Verify that the barrier is completely closed by making sure that the wiring compartment is isolated from the bus compartment.

Right Panel (Side View)

Wireway Area

Horizontal Bus Area

Installing the Right Panel into the Rear Groove

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?