80459-641-01, Rev. 09

Units Below the Topshelf

If applicable, remove the plug-in unit below the topshelf (see Remove Existing Brackets on the 15 in. (381 mm) Deep MCC).

Refer to either the Model 5 MCC Installation and Maintenance Manual (# 8998IM9101R5/92) or Removing the Control Unit of this bulletin for unit removal instructions. If necessary, contact your local Schneider Electric field sales representative to obtain this bulletin.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?