Adjusting Mag-Gard, PowerPacT, or TeSys Magnetic Trip Setting
The adjustable magnetic trip setting is factory-set at Lo for Mag-Gard Motor Circuit Protectors. For PowerPacT H- and J-frame, and TeSys BV4 Motor Circuit Protectors, where applicable, the Full Load Amp Setting (FLA) is factory set to the lowest setting. The instantaneous trip setting (Im) is factory set to the Auto 1or the lowest instantaneous trip setting. For PowerPacT P-frame Motor Circuit Protectors (ET1.0M electronic trip unit), the adjustable instantaneous trip setting is factory set to its lowest position. These settings may have to be adjusted for proper motor start-up. For Mag-Gard, PowerPacT, and TeSys BV4 Motor Circuit Protectors, refer to the magnetic trip set-point limits outlined in the applicable national installation codes. For PowerPacT H- and J-frame Motor Circuit Protectors, refer also to instruction bulletin 48940–260–01, Motor Circuit Protector (MCP) Settings For PowerPact H- and J-frame Motor Circuit Protectors .
![]() |
---|
Hazard of Electric Shock, Explosion, or Arc Flash
Failure to follow these instructions will result in death or serious injury.
|
To access the MagGard trip or TeSys BV4 adjustment dial:
-
Turn off all power supplying this equipment before working on or inside the equipment, and follow lockout/tagout procedures. Always use a properly rated voltage sensing device to confirm the power is off.
-
Place the unit handle in the OFF position and open the door.
-
While pushing the door interlock lever forward, trip the circuit breaker by pressing the test button (see Mag-Gard and TeSys BV4 Magnetic Trip Adjustment). The disconnect handle will automatically move up, allowing access to the adjustment dial.
After obtaining the motor full load current from the motor nameplate, select an adjustable trip setpoint to test start the motor. Further adjustments may be required because of motor load characteristics. Refer to applicable national installation codes for permissible setpoints.
After adjusting the trip setting, reset the circuit breaker by moving the disconnect handle to the ON position and then to the OFF position.
To access the PowerPacT H- and J-frame Full Load Amps (FLA) and Instantaneous Trip setting (Im) dials:
-
Turn off all power supplying this equipment before working on or inside the equipment, and follow lockout/tagout procedures. Always use a properly rated voltage sensing device to confirm the power is off.
-
Place the unit handle in the OFF position and open the door.
-
To set the FLA and Im dials, refer to instruction bulletin 48940–260–01, Motor Circuit Protector (MCP) Settings For PowerPact H- and J-frame Motor Circuit Protectors.
-
Select replacement MagGard, PowerPacT, or TeSys BV4 Motor Circuit Protectors for MCCs using the voltage and current ratings listed in the Model 6 MCC Catalog (8998CT9701) in addition to the Mag-Gard, PowerPacT, or TeSys selection tables in the Schneider Electric Digest.
-
These circuit breakers are suitable for motors with locked-rotor indicating code letters based on applicable national codes and standards. For other motors, consult your local Schneider Electric field sales representative.
To access the PowerPacT L-frame trip adjustment dial (Isd):
-
Turn off all power supplying this equipment before working on or inside the equipment, and follow lockout/tagout procedures. Always use a properly rated voltage sensing device to confirm the power is off.
-
Place the unit handle in the OFF position and open the door.
-
Set the overcurrent trip setting by adjusting the switch labeled "Isd" as shown in PowerPacT L-frame Instantaneous Trip Adjustment. The dial is labeled in amperes. Refer to instruction bulletin 48940–310-01, MicroLogic™ 0, 1, 2, and 3 Trip Units—User Guide, for more information on trip settings.
After obtaining the motor full load current from the motor nameplate, select an adjustable trip set-point to test start the motor. Further adjustments may be required because of motor load characteristics. Refer to applicable national installation codes for permissible set-points.
To access the PowerPacT P-frame Instantaneous Trip setting (Im) dial:
-
Turn off all power supplying this equipment before working on or inside the equipment, and follow lockout/tagout procedures. Always use a properly rated voltage sensing device to confirm the power is off.
-
Place the unit handle in the OFF position and open the door.
-
Make adjustments as follows:
-
For ET1.0I and ET1.0M electronic trip units, adjust instantaneous trip (Ii) by adjusting switch A (see PowerPacT P-frame Instantaneous Trip Adjustment). Switch settings are multiples of the frame rating.
-
For P-frame MCPs with other Micrologic electronic trip units, see instruction bulletin 48049-148-05, PowerPact™ P-Frame and NS630b–NS1600 Circuit Breakers
-
After obtaining the motor full load current from the motor nameplate, select an adjustable trip set-point to test start the motor. Further adjustments may be required because of motor load characteristics. Refer to applicable national installation codes for permissible set-points.