80459-641-01, Rev. 09

Joining Corner Channels

Hardware Kit

  1. Turn off all power supplying this equipment before working on or inside the equipment, and follow lockout/tagout procedures. Always use a properly rated voltage sensing device to confirm the power is off.

  2. The hardware kit for joining sections (see Hardware Kit) is bagged and tied to the right front corner channel of each shipping split.

  3. Locate the four half-circle shaped notches on the inside surface of the corner channels (see Bolting Sections Together, View A).

  4. Using four of the 3/4 in. x 1/4-20 hex head thread-forming screws supplied in the hardware kit, join the front vertical corner channels by inserting the screws through the clearance holes located within the halfcircle shaped notches and into the mating threadforming hole (see Bolting Sections Together, View B).

    NOTE: Insert the screws from whichever side provides the easiest access to the holes; either side will allow proper joining of the channels.
  5. Tighten the screws (see Bolting Sections Together, View C).

  6. Repeat steps 3–5 to connect the rear corner channels.

NOTE: In some instances, holes in the rear channels will only be accessible from the rear of the MCC with the MCC back plates removed. If the MCC is not rear accessible, install as many screws as possible from the front of the MCC (typically via the vertical wireway).

Bolting Sections Together

View A

View B

View C

View D: Front Bottom Side Channel Connection

View E: Rear Bottom Side Channel Connection

View F: Top Front Side Channel Connection

View G: Top Rear Side Channel Connection (Shown with MCC back plates removed.)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?