80459-641-01, Rev. 09

Removal

  1. Turn off all power supplying this equipment before working on or inside the equipment, and follow lockout/tagout procedures. Always use a properly rated voltage sensing device to confirm the power is off.

  2. With one hand, slide the left panel to the right until it unsnaps from the right panel.

  3. Align the arrows on the left panel and top track as shown in Aligning the Arrows on the Panels. Lift the panel out of the bottom track, and remove the panel.

  4. Align the arrows on the right panel and top track as shown in Aligning the Arrows on the Panels. Lift the panel out of the bottom track, and remove the panel.

Aligning the Arrows on the Panels

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?