80459-641-01, Rev. 09

Plug-In Units

Some MCC units can weigh up to 200 pounds and require two or more persons or special handling equipment. Lift only by supporting bottom and/or side panels of the unit. Refer to Proper/Improper Lifting Points for Plug-in Units Taller Than 24 in..

Proper/Improper Lifting Points for Plug-in Units Taller Than 24 in.

Proper Lifting Points

Improper Lifting Points

Before installing any MCC control units, locate and retighten or retorque any connections that may have loosened during shipment and handling. Refer to the procedures in Installing Additional MCC Units.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?