80459-641-01, Rev. 09

Tie-Down Points for Rigid, Floor-Mounted Equipment

The equipment enclosure provides anchorage tie-down points to accept anchor attachments to the building structure or foundation. Model 6 MCC indoor enclosures provide enclosure base frame clearance holes for bolted anchorage attachments, as shown in the figures Type 1, Type 1 Gasketed, Type 1 Sprinkler Resistant, and Type 12 Seismic Tie Down Locations and Seismic Tie-Down Locations for 18-Pulse AC Drive MCC Sections. Model 6 MCC outdoor enclosures provide enclosure base frame clearance holes for bolted anchorage attachments, as shown in the figure Type 3R Seismic Tie-Down Locations.

MCC sections must be anchored using all enclosure tie-down points, as shown in the figures referenced above, for indoor and outdoor applications.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?