Modifying Fixed Units
-
Turn off all power supplying this equipment before working on or inside the equipment, and follow lockout/tagout procedures. Always use a properly rated voltage sensing device to confirm the power is off.
-
If drilling holes in the back of the MCC unit saddle is required, do not drill through the back of the saddle more than 0.1875 in. (5 mm). Use a drill stop device for this procedure.
-
Perform the required modifications. Use thread-forming screws to mount devices. Do not use bolts and nuts, as they could loosen over time and cause property damage or personal injury. The hardware must not extend beyond the back of the MCC unit saddle more than 0.25 in. (6 mm) or beyond the sides and bottom pan by more than 0.125 in. (3 mm).
-
Maintain proper electrical spacings * in the unit.
-
Use a vacuum cleaner to remove all debris left in the unit as a result of the modifications. Do not use compressed air to blow out the unit, because all debris may not be fully removed.
-
Perform the recommended maintenance procedures beginning in Maintaining the Control Unit of this manual.
-
Use a megohmmeter to perform an insulation test as outlined in Insulation Test.
-
Follow the procedures for Energizing the MCC.