80459-641-01, Rev. 09

Remove Existing Components

Follow these instructions to remove the existing top horizontal wireway cover, bus barriers, units below the topshelf, and brackets [15 in. (381 mm) deep MCC]:

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?