80459-641-01, Rev. 09

Anchorage Assembly Instructions

The bolted anchor assembly view depicted in the figure Bolted Anchor Assembly illustrates the equipment’s as-tested attachment to a seismic shake-table test fixture. The equipment seismic capacity, as stated on the Schneider Electric CoC, was achieved with the identified size and grade attachment hardware. For bolted attachments, the use of factory-supplied Belleville conical spring washers at specified locations is required to maintain seismic conformance. Field installed equipment attachment and support detailing must be in accordance with the anchorage system requirements as defined by the construction site structural engineer, registered design professional, or engineer of record.

Bolted Anchor Assembly

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?