80459-641-01, Rev. 09

Splice to Existing Left

  1. Turn off all power supplying this equipment before working on or inside the equipment, and follow lockout/tagout procedures. Always use a properly rated voltage sensing device to confirm the power is off.

  2. Remove the end plate and all flat gaskets from the existing MCC. Leave the P gasket on the existing front corner channel in place.

  3. Remove the factory installed flat gasket from the front corner channel of the new vertical section.

  4. Join sections together following the appropriate steps in Joining Type 1, Type 1 Gasketed, and Type 12 Sections or Joining Type 1 Sprinkler-Resistant Sections.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?