80459-641-01, Rev. 09

Retrofit Brackets and Endcaps

Follow the applicable instructions below to install retrofit brackets into 15 in. (381 mm) or 20 in. (508 mm) deep MCCs. The top retrofit bracket must sit flush against the side channel. Slide the black grommets toward the back of the MCC.

  • 15 in. (381 mm) deep MCC: Use a rivet gun and two rivets in the retrofit kit to attach the retrofit brackets to the left and right side channels (see 15 in. (381 mm) Deep MCC Retrofit Bracket).

  • 20 in. (508 mm) deep MCC: Use the screws provided in the retrofit kit to attach the retrofit brackets to the left and right side channels. Align the holes in the bracket and side channel as shown in 20 in. (508 mm) Deep MCC Retrofit Bracket.

NOTE:
  • Even if the holes are present for a direct mounting of the endcap to the side channels, use the top retrofit bracket on 20 in. (508 mm) deep MCCs.

  • Before tightening the screws, push the bracket away from you so that the rear bracket hole is properly aligned with the side channel hole.

15 in. (381 mm) Deep MCC Retrofit Bracket

20 in. (508 mm) Deep MCC Retrofit Bracket

Follow the steps below to install the endcaps (see Endcap Placement).

  1. Rivet one endcap into place on the retrofit bracket or the side channel, either to the right or left side of the structure.

  2. Insert one end of the top track into the attached endcap.

  3. Place the other endcap on the opposite end of the top track, and slide the top track into place.

  4. Rivet the second endcap to the retrofit bracket.

Endcap Placement

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?