80459-641-01, Rev. 09

Conductor Entry for Line-Side Isolation Cable Vaults with ArcBlok

Conduit entry into main breaker sections equipped with ArcBlok and line-side Isolation cable vaults will require:

  • Use of an 18 in. pull box for top-feed entry with a removable top plate.

  • Line-side isolation cable vaults will require removal of enclosure covers and barriers prior to removing the cable vault front cover and ArcBlok lug cover.

Line-Side Isolation Cable Vault and ArcBlok Top-Feed Main Breaker Access

Line-Side Isolation Cable Vault and ArcBlok Top-Feed Main Lug Breaker Access

Line-Side Isolation Cable Vault and ArcBlok Bottom-Feed Main Breaker Access

Line-Side Isolation Cable Vault and ArcBlok Bottom-Feed Main Lug Breaker Access

NOTE: Cable entry into line-side isolation cable vaults must use conduit connection means installed on the closing plate (in bottom-feed applications) or the pull box top closing plate (in top-feed applications). Conduits must be sealed using duct seal putty.

Line-Side Isolation Cable Vault Conduit Installation and Sealing

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?