80459-641-01, Rev. 09

Motor Logic Retrofit Applications

DANGER
Hazard of Electric Shock, Explosion, or Arc Flash
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E, NOM-029-STPS-2011, or CSA Z462.
  • This equipment must only be installed and serviced by qualified electrical personnel.
  • Turn off all power supplying this equipment before working on or inside equipment.
  • Always use a properly rated voltage sensing device to confirm power is off.
  • Replace all devices, doors, and covers before turning on power to this equipment.
Failure to follow these instructions will result in death or serious injury.
NOTICE
incorrect operation
  • Lug Kits:
    Use only 9999 LBO and 9999 LLO purchased after 5/1/95 for Size 0, 00B, 00C, and Size 1 units.
  • Z Element:
    Do not use the 9999Z3, 9999Z2, or 9999Z1 developed for open and general enclosed starters.
Failure to follow these instructions can result in equipment damage.

Remove the starter from the unit to replace the overload (melting alloy/bi-metallic). See Removing the Control Unit.

Terminal blocks (OEKTTBML) should be used for applications requiring multiple passes to achieve the proper adjustment range.

Restrain looped load cabling between the overload and the terminal block with wire ties or the equivalent when terminal kits are used.

On Size 3 and 4 starter units, the overload reset button is 1-5/8 in. (41 mm) further from the unit door and may require an alternative reset assembly (80420-862-51).

Retrofitting NEMA rated Compac 6, six-inch (52 mm) units is not recommended. The Motor Logic overload relay is available factory installed in Compac 6.

On 600 V Size 1 applications, add a third wire tie between the circuit breaker and contactor near the contactor line lugs. Refer to instruction bulletin 30072-013-29 for additional information.

NOTE: For retrofit applications, contact your Schneider Electric field sales representative for assistance. Schneider Electric assumes no responsibility for the design or implementation of retrofits unless contracted to perform them.

Use copper wire only on device power and control terminals. Conductors must be sized for 60°C or 75°C National Electrical Code® (NEC®) ratings.

Pressure wire terminals are suitable for wire sizes #16–12 AWG, solid or stranded. Terminal instruction labels are located adjacent to the terminal block or on the wireway door.

Box lugs (on interposing power terminal blocks supplied with selected units) are suitable for wire sizes #14–8 AWG, solid or stranded. Terminal instruction labels are located adjacent to the terminal block. Lug Types and Wire Sizes provides additional termination data.

Lug Types and Wire Sizes

Class 9065 Motor Logic Overload Relay Size* Rating Lug Type Wire Size* Torque Values*
00B 1.5–4.5 A Pressure Wire* 14–8 AWG (2.5–6 mm2) 25 lb-in
(2.8 N•m)
00C 3–9 A Pressure Wire* 14–8 AWG (2.5–6 mm2) 25 lb-in
(2.8 N•m)
0 6–18 A Box Lug 14–4 AWG (2.5–16 mm2) 50 lb-in
(5.6 N•m)
1 9–27 A Box Lug 14–4 AWG (2.5–16 mm2) 50 lb-in
(5.6 N•m)
3 30–90 A Box Lug 14–1/0 AWG (2.5–50 mm2) 100 lb-in
(11.3 N•m)
4 45–135 A Box Lug 8–250 MCM (6–120 mm2) 200 lb-in
(22.6 N•m)
5 90–270 A Box Lug 250–500 MCM (120–240 mm2) 250 lb-in
(28.2 N•m)
6 180–540 A Clamp Lug 250–500 MCM (120–240 mm2) 375 lb-in
(42.4 N•m)

Size 00B, 00C, 0, and 1 relays have conductor (CT) windows through which the motor leads must pass before being connected to the load terminals on the contactor (T1, T2, and T3). By allowing multiple passes (turns) of the load leads through these CT windows, overload protection can be provided for motors with a full-load current lower than the specified operating range.

Two passes of the load leads through each window effectively increase (by a multiple of two) the current that the overload relay senses. Three passes effectively increase the current by a multiple of three. All three conductor windows must have the same number of passes, looped in the same direction, for the overload relay to operate properly (see Looping Passes).

Looping Passes

Passes should begin from the load side of the overload through the CT window and return via the windows provided between the baseplate and overload (see Motor Logic Overload (Bottom View)). The final pass terminates on the load side of the contactor.

MCC units requiring multiple passes are factory supplied prelooped with #14 AWG wire and interposing terminal blocks. Refer to for information concerning retrofit.

Motor Logic Overload (Bottom View)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?