80459-641-01, Rev. 09

Horizontal Wireway Cover

  1. Turn off all power supplying this equipment before working on or inside the equipment, and follow lockout/tagout procedures. Always use a properly rated voltage sensing device to confirm power is off.

  2. Remove the screws that secure the top horizontal wireway cover to the structure, and then remove the cover.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?