80459-641-01, Rev. 09

Existing Brackets: 15 in. (381 mm) Deep MCC Only

If the MCC is 15 in. (381 mm) deep, use a 1/8 in. (3 mm) drill bit to remove the rivets that hold the right and left horizontal bus barrier brackets in place (see Remove Existing Brackets on the 15 in. (381 mm) Deep MCC). Discard the brackets after removal.

NOTE: Discard all retrofit brackets if the existing bus barrier bracket “B” (see Remove Existing Brackets on the 15 in. (381 mm) Deep MCC) is present on the 15 in. (381 mm) deep MCC. All holes are already present for direct mounting of the horizontal bus barrier.
DANGER
Hazard of Electric Shock, Explosion, or Arc Flash
  • Drilling increases the chance of loose particles in the MCC.
  • Confirm that the compartment is free of loose particles before turning on power to this equipment.
Failure to follow these instructions will result in death or serious injury.

Remove Existing Brackets on the 15 in. (381 mm) Deep MCC

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?