80459-641-01, Rev. 09

Water-Sprayed or Splashed MCC (Clean Water Only)

DANGER
Hazard of Electric Shock, Explosion, or Arc Flash
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E, NOM-029-STPS-2011, or CSA Z462.
  • This equipment must only be installed and serviced by qualified electrical personnel.
  • Turn off all power supplying this equipment before working on or inside equipment.
  • Always use a properly rated voltage sensing device to confirm power is off.
  • Replace all devices, doors, and covers before turning on power to this equipment.
Failure to follow these instructions will result in death or serious injury.

If the MCC has been sprayed or splashed with small amounts of clean water, make a thorough inspection of the entire system and verify that no damage to conductors or insulation has occurred. Do not open sealed devices such as molded case circuit breakers or fuses. Replace these devices if they are damaged. Refer to the appropriate instruction bulletin listed in MCC-Related Literature.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?