80459-641-01, Rev. 09

Power Bus Splicing MCCs with Multiple Bar/Phase Splice Kit

NOTE: On the integral splice bar assembly, located on the left side of each phase bus, the number of splice bars used on each phase is one greater than the number of main horizontal bus bars. The rear-most splice bar includes captive nuts.
  1. Remove the two left bolts. Loosen, but do not remove, the two right bolts on the splice assembly (see Remove the Left Bolts and Loosen the Right Bolts on the Splice Assembly).

    NOTE: Do not remove the two right bolts from the splice assemblies. Doing so will permit spacers to fall from the splice assembly. If this occurs, re-assemble the splice bars and spacers (if applicable) in the proper order before continuing.

    Remove the Left Bolts and Loosen the Right Bolts on the Splice Assembly

  2. Slide the splice assembly to the left until the two left holes are in line

    with the corresponding holes in the horizontal bus on the left section (see Align the Splice and Bus Holes).

    Align the Splice and Bus Holes

  3. Reinstall the two left bolts through the splice bars and into the horizontal bus (see Insert the Splice Bolts); make sure the original conical washers are reinstalled with the concave side facing the splice bus (see Place a Conical Washer Under the Bolt Head).

    Insert the Splice Bolts

    Place a Conical Washer Under the Bolt Head

  4. Torque all bolts on both ends to 31–32 lb-ft (41.87–43.22 N•m) (see Torque the Bolts).

    Torque the Bolts

  5. Return to Step 2 in for all phases and for the neutral bus (if supplied). When all splices are complete, go to Step 6.

  6. Before energizing the equipment, slide the horizontal bus barriers into the closed position and replace all covers.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?