80459-641-01, Rev. 09

Motor Logic Plus Local Programming

DANGER
HAZARd of electric shock, explosion, or Arc Flash
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E, NOM-029-STPS-2011, or CSA Z462.
  • Turn off all power supplying this equipment before working on or inside the Motor Control Center.
  • Use a properly rated voltage sensing device to confirm that all power is off. Control units must be de-energized before performing maintenance on the MCC.
  • The unit disconnect switch must be locked in the “off” position before working on equipment.
Failure to follow these instructions will result in death or serious injury.

Local programming can be used for Motor Logic Plus setpoint programming and detected error readout purposes. Verify that the display is unlocked (the default setting), and disconnect all power before performing the steps below to accomplish local programming:

  1. Turn off all power supplying this equipment before working on or inside the equipment, and follow lockout/tagout procedures. Always use a properly rated voltage sensing device to confirm the power is off.

  2. Connect a 9 V supply to the “P” and “G” terminals using the supplied connector, Schneider Electric part # 80445-519-50 (see Motor Logic Plus Communication Module Terminals).

    Motor Logic Plus Communication Module Terminals

  3. Turn the “Mode Select” switch to the parameter you are programming. Refer to Schneider Electric instruction bulletin 30072-013-98_ (see iMCC-Related Literature) for a list of parameters.

  4. Press and hold the “Reset/Program” button.

    NOTE: The display will not illuminate for local programming if the “Mode Select” switch is in the “Run” position.
  5. Turn the “Display/Program” dial to the desired setting as shown on the LED display.

  6. Release the “Reset/Program” button.

  7. Turn the “Mode Select” switch back to the “Run” position.

  8. Disconnect the 9 V supply and its connector.

Messages are displayed on the 3-digit LED display when harmful conditions are detected. Local Message Display contains a list of the message codes and their definitions.

Local Message Display

Displayed Message Meaning
oc Tripped on over current
SP Tripped on single phasing
ub Tripped on voltage or current unbalance
uC Tripped on under current
cF Tripped on contactor misoperation
GrF Tripped on ground fault
HI Tripped on over-voltage
Lo Tripped on under-voltage
rP Incoming phases have been reversed
oFF A stop command was issued from a remote source
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?