HRB1684301-16

Access levels

You can set the level of access for each configured IP address, as well as for anonymous IP addresses.
Access level Description
Read-only This setting allows only the following function codes to be sent to the meter and any downstream serial devices from the specified IP address: 01 (0x01), 02 (0x02), 03 (0x03), 04 (0x04), 07 (0x07), 08 (0x08), 11 (0x0B), 12 (0x0C), 17 (0x11), 20 (0x14), 24 (0x18), 43 (0x2B) and 100 (0x64)
Full This setting allows any Modbus function code to be sent to the meter and any downstream serial devices from the specified IP address.
None This setting denies access to anonymous IP addresses.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?