Data display and analysis tools
- Power Monitoring
ExpertEcoStruxure™ Power Monitoring Expert is a complete supervisory software package for power management applications.
- Power
SCADA Operation EcoStruxure™ Power SCADA Operation is a complete real-time monitoring and control solution for large facility and critical infrastructure operations.
- Building OperationStruxtureware™ Building Operation is a complete software solution for integrated monitoring, control, and management of energy, lighting, fire safety, and HVAC.
- Modbus command interfaceMost of the meter’s real-time and logged data, as well as basic configuration and setup of meter features, can be accessed and programmed using a Modbus command interface as published in the meter’s Modbus register list.
- Meter Insights and QR code-enabled metersThe QR code feature allows you to view meter data using the Meter Insights website by scanning a QR code on the meter’s display.
Parent topic: Meter overview